Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM350 FAQ GPIOs and Pinmuxing
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM350 FAQ GPIOs and Pinmuxing

Q: How many GPIOs are available in ADuCM350?

A: Up to 66 depending on peripheral function use. Each GPIO can be configured as an input or an output.

They also have internal pull-up or pull-down programmable resistors. All I/O pins are functional over the full supply range (VBAT = 1.8 V to 3.6 V), and the logic input voltages are specified as percentages of the supply.

Q: Can the LCD segment driver pins be configured as GPIOs?

A: Yes. One important note is that these pins are on the VLCDVDD supply domain. When the segment driver is not being used, the VLCDVDD pin should be connected to VCCM in order to power the P1.X and P2.X GPIO pins. See LCD Charge Pump and External Capacitor Requirements section of the ADuCM350 Hardware Reference Manual (UG-587).

Q: How do I mux different peripherals on the GPIO pins?


A: A Pin Multiplexing application (PinMuxUI) is provided as part of the Software Development Kit (SDK) which is capable of generating code to set all of the port MUX and FER registers statically for all peripherals in a single call. Further information can be found in the the Build Configurations chapter of the ADuCM350BBCZ Software User's Guide. The application can be found in the tools directory of the SDK installation.

Q: Can I use P1.7 (CLKOUT) as a Clock Source for an external device ?

A:

Device Considerations:

  • Pad B8 (P1.7/S10/D7) is always supplied by VLCD rail, regardless if LDC logic is enabled
  • Pad mux can be changed from LCD to GPIO, PDI or CLKOUT
  • VLCD rail supports 2 use cases: direct connection to battery (VCCM) and generation from internal charge pump
  • If enabled, the VLCD charge pump can continuously deliver 200 uA (2.4V to 3.6V)
  • If GPIO or alternate pin function is enabled while LCD charge pump is enabled, the following limitations apply:
  • VOL/VOH and VIL/VIH will track VLCD supply – datasheet specs are not applicable in this operating mode
  • I/O drive strength as described in datasheet is not applicable in this operating mode
  • Drive strength register should never be set high in this operating mode

LOAD Considerations If Using LCD and P1.7 for Clock Source

  • Multiplexed mode can drive up to 32 FP and 4 BP = 128 Segments, but only 32 are driven at a time and FP – BP < VLCD
  • Worst case is static mode: FP – BP = VLCD
  • VDC (average) = 0 VDC
  • Vrms = VLCD
  • Worst case refresh ratio = 80 Hz
  • Worst case capacitance of a segment = ~130 pF
  • Segment impedance has no resistive component; only reactive:
  • Z=X_C=1/((2πfC) )=1/((2π×80×130E-12) )=1.53E+7Ω
  • I=V/Z=(3.0V)/(1.53MΩ)=196nA
  • Maximum 32 segments: 32×196nA=6.3uA
  • VLCD load due to LCD glass is negligible

Headroom Analysis (assume external device requires 32kHz clock)

  1. To allow sufficient headroom for corner cases, avoid continuous load on VLCD > 100 uA
  2. Current available for Device Clock ~ 100 uA
  3. Minimum resistive divider: R=V/I=(3.0V)/100uA=30K
  4. Adding a resistive divider to clock output creates an RC network with External Device clock circuit input capacitance
  5. Cutoff frequency 〖=f〗_c=1/2πRC
  6. Use lowest value resistive divider allowed given current available
  7. If R=30K, then f_c=1/((2×π×30000×50E-12) )≅106kHz
  8. f_c>3X External Device Clock

Added Considerations

  • If LCD contrast (adjustment of VLCD bias) is used, equations in headroom analysis must be adjusted
  • If VLCD bias is adjusted, VOL/VOH will track and may have implications in RC network created by voltage divider and External Device clock input capacitance
  • Temperature and process variations in resistive divider may influence effective jitter on clock output signal used for External Device
  • Pad B8 (P1.7/S10/D7) configured as CLKOUT will not operate when the device is in hibernate (DEEPSLEEP)
Tags: aducm350 lcd gpio vlcdvdd aducm35x p2.x p1.x Show More