Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM350 FAQ AFE / ADC Measurement Channel
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM350 FAQ AFE / ADC Measurement Channel

Q: How to calculate current resolution ?

A: Input Current Resolution = 3.6V/2^16 x 1/1.5 x 1/RTIA = 14.6nA (assumption RTIA=2.5kΩ as in diagram below )

Q: Can I do a differential measurement using ADC Mux.

A: Yes. Use the P-N channel option. The caveat is that you have AFE pins available to switch the P and N channels out.The excitation buffer and IN-amp should be powered down in the AFE Sequence during the P-N measurement.

Q: What are the data update rates ?

A:

  • If using the DFT then a Real and Imaginary component of the impedance is available every 12.8mS.
  • If using PSR filter settling time is 900SPS.
  • Raw ADC data is available at 160KSPS - This is FIXED - no configurability. If other sample rate required the raw data can be averaged in Core.

Q: Dynamic Range of ADC ?

A: Typically 95 dB

Q: Details on precision specifications ?

A: See ADuCM350 Datasheet.

Q: What is the maximum common mode ? ADC input range ? Etc

A: Please refer to the "AFE Signal Swings" section in AFE Excitation Loop chapter of UG-587 and the ADC Measurement section

in ADC Chapter of UG-587.

Q: Hoe much current can you sink into load ?

A: Typically 5mA.

Q: What is Non-Coherent Sampling ?

A: Example scenarios is where the DAC and ADC are clocked st 160KHz. The images of the excitation frequency can be aliased back into the same FFT bin as the fundamental. By developing a non-choherent excitation signal by changing the DAC update rate you prevent the aliased images from falling inside this fundamental bin.

Q: Why should I only use 1/8 to 7/8 of the ADC and DAC available ranges?

A:The rest of the range is used in the autocalibration sequnces to remove offset and gain effects. See No Factory Cal chapter in UG-587.

Q: I am measuring 1/2VCCMANA through the ADC MUX selector. With a 3V VCCM at pin I am measuring ~2.87 V. Why the disparity ?

A:  To divide down the VCCM signal by 2 a potential divider is used (R1 and R2). These resistors have limited matching capability which allows for an accuracy spec of 1% for all of these general monitoring functions on the ADC Mux.

Tags: adc loop aducm350 afe aducm35x