Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Bioimpedance Measurement Using ADuCM350
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Bioimpedance Measurement Using ADuCM350

Setup

Note this is an example "reference" to setup the ADuCM350 for 4-Wire Skin impedance measurements.

4-Wire measurements are for Absolute Accuracy and the ADuCM350 requires an external In-Amp.

For Relative measurements, the ADuCM350 can operate as a single chip solution.

Review AN-1302 for the differences between 2-Wire Skin Impedance and 4-Wire Skin Impedance. AN-1271 is useful to optimize the ADuCM350 Impedance engine for optimal performance.

  • Documentation: AN-1302, and Configuring ADuCM350-BIO3Z board for 50kHz Bio-Impedance Measurement.pdf
  • Hardware
    • Eval-ADuCM350EBZ (LK1 is in place)
    • ADuCM350 4Wire Bio Config 3 (Eval-ADuCM350BIO3Z) board. (LK7, LK8, LK9, LK10 in place; LK16, LK17, LK18, and LK19 in position B)
  • Software
    • ImpedanceMeasurement_4WireBioIsolated_BodyComp example in IAR Embedded Workbench
  • View data in Comms port / Terminal IO (Check SDK Userguide in document folder for details).

Note: When performing the Bio-Impedance measurement on the body, please ensure the laptop is unplugged from the power source as an additional precaution.

SDK Download /Debug and Collect Data

  • Download and Debug Code
    • As Per SDK Quickstart UG-677
  • In default mode 1.5KOhm is selected.
    • See 4-Wire Bio Config 3 schematic and layout.
  • Theory / System connections  documented in detail on AN-1302 apps note
  • Once Code is Download -> Run Code and view data in Terminal I/O or UART.
  • Should get results below out of box for default settings.

Validate Results

  • Hardware Change: Connect LK16, LK17, LK18, and LK19 in position A. insert USB-mini Cable, stripped at the other end, and connect the impedance to be measured at the stripped end.
  • Repeat Measurement.
    • Hit Reset and then Run buttons
    • You should see impedance connected in the stripped end  of the USB-mini cable in results display.

Data View

The raw DFT complex results (real and imaginary parts) and the final calibrated unknown impedances (represented in polar coordinates; magnitude and phase) are reported through the UART/STDIO. The USE_UART_FOR_DATA macro determines whether the results are returned to the UART or STDIO.

To return data using the UART, set the macro USE_UART_FOR_DATA = 1 (this is the default option).

To return data using STDIO, set the macro USE_UART_FOR_DATA = 0.

Attachments:
ImpedanceMeasurement_4WireBioIsolated_BodyComp.zip
3113.attachment.pdf
BIO3ZBoardSchematic.pdf
Tags: aducm350 aducm35x bioelectric impedance biomedical bioimpedance skin impedance Show More