Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor

4-Wire-Bio-Config 3 Board

  • Used to measure a matrix of ideal R and C components.
  • Has built in USB-micro connector to measure “real world” sensors.
  • Please refer to 4-Wire Bio Config 3 Layout and Schematic in Design Documentation folder when evaluating and modifying board.

Step 1: Validate Board with Software

  • Measure 1.5K (1% accurate) resistor
    • Insert following Links:LK7,LK8,Lk9,LK10
    • Insert Links LK16, LK17, LK18, and LK19 on Position B.

Step 2: Electrode Hook Up

  • Using the “4-Wire Bio Config 3” board, insert a USB-micro cable with stripped end on the other side.
    • Rlimit resistor and Isolation capacitors will need to be maintained in signal chain to meet IEC standards.
    • Raccess will need to be removed from measurement.
  • Insert following Links: LK7,LK8,Lk9,LK10.
  • Insert following Links on Position A: LK16,LK17,Lk18,LK19.

4-Wire-Isolated Electrode Configuration

Block Diagram

Insert following Links: LK7, LK8, LK9 and LK10. 

Board Pictures

Tags: aducm350 aducm35x bioimpedance
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • Comment on 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    mtabboud
    Fisrt I want to thank you for the detailed description but lLooking at this document, i feel something is wrong?? Under Step 1 you are asking to insert " Insert following Links:LK7,LK8,Lk9,LK10,LK12 and...
  • Bioimpedance Measurement Using ADuCM350
    GenevaC
    Setup Note this is an example "reference" to setup the ADuCM350 for 4-Wire Skin impedance measurements. 4-Wire measurements are for Absolute Accuracy and the ADuCM350 requires an external In-Amp. ...
  • RE: 4-wire Isolated Bioimpedance real world problem
    Yongshengliu
    Hi Liam, Thanks for your respose. 1. 4-Wire Bio board configuration check 2. Plot of above setting 3. The external connection just follow the description in the https://ez.analog.com/docs/DOC...
 
Related Content
  • Comment on 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    mtabboud
    Fisrt I want to thank you for the detailed description but lLooking at this document, i feel something is wrong?? Under Step 1 you are asking to insert " Insert following Links:LK7,LK8,Lk9,LK10,LK12 and...
  • Bioimpedance Measurement Using ADuCM350
    GenevaC
    Setup Note this is an example "reference" to setup the ADuCM350 for 4-Wire Skin impedance measurements. 4-Wire measurements are for Absolute Accuracy and the ADuCM350 requires an external In-Amp. ...
  • RE: 4-wire Isolated Bioimpedance real world problem
    Yongshengliu
    Hi Liam, Thanks for your respose. 1. 4-Wire Bio board configuration check 2. Plot of above setting 3. The external connection just follow the description in the https://ez.analog.com/docs/DOC...