Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM350 FAQ AFE TIA
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM350 FAQ AFE TIA

Q: What is the maximum common mode ? ADC input range ? Etc

A: Please refer to the "AFE Signal Swings" section in AFE Excitation Loop chapter of UG-587 and the ADC Measurement section

in ADC Chapter of UG-587.

Q: Details on main TIA specifications such as noise drift.

A:

  • Gain/Offset Calibration on power up.
  • Offset Calibration with respect to 0uA input current ( leakage current from switch matrix calibrated out )
  • TIA_O is sensed with respect to TIA_I (not VBIAS) so TIA OpAmp offset drift and noise rejected

Q: Can I adjust the Common Mode / VBIAS of the TIA ?

A:The default configuration for the common mode of the TIA is 1.1V or set by the VBIAS buffer. The part is characterised and tested with this common mode value. However it is possible to change the common mode voltage.

As figure shows below, use a potential divider off the REF_EXCITE pin to control the VBIAS from a default of 1.1V.

Be aware of the measurement channel rails when adjusting the common mode.

It is possible to make this Common Mode Software configurable by adding a resistor between VREF and VBIAS. In this case:

  • REF_EXCITE = 0 and VBIAS-BUF_EN = 1 for Default option where VBIAS = 1.1V.
  • REF_EXCITE = 1 and VBIAS_BUF = 0 for user desired Common Mode level.

Tags: vbias aducm350 aducm35x tia
  • Share
  • History
  • More