Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents FAQ ADuCM350 Embedded Software Development
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

FAQ ADuCM350 Embedded Software Development

Q: How do I get the ADuCM350 Software Development Kit (SDK)? How much does it cost?

A: The SDK can be downloaded from the ADuCM350 product page. There is no charge to download the SDK.

Q: What tool chains are currently supported by the Software Development Kit (SDK)?

A: At this time only the IAR Embedded Workbench for ARM (EWARM) Cortex-M tool chain is supported by the SDK. The minimum version requirement for v2.2.0.0 of the SDK is EWARM v7.1.

Q: I dowloaded and installed the SDK, then I downloaded and installed EWARM, but when I try to build any of the SDK examples, I keep getting errors, what should I do?

A: The SDK installer will install some important configuration files to the EWARM directory. If you install the SDK before EWARM, the IDE will not be able to find these files which will generate build-time errors. EWARM should be installed before the SDK. If you have already installed these in the wrong order, re-run the SDK installer, ensuring that you select the version of EWARM that you are using.

Q: Do I need the full version of the IAR EWARM?

A: The code size limited or time limited kickstart version of EWARM will be sufficient for the compilation and download of all SDK examples, except for those which use the Micrium µC/OS-II RTOS or the Micrium USB stack. For these examples, the code size limited version of EWARM will not be sufficient.

Q: Does the SDK provide Real-Time Operating System (RTOS) support?

A: The Micrium µC/OS-II is supported by the SDK. The various peripheral drivers use a conditional compilation macro which enables RTOS support. Note that ADI does not deliver the Micrium source files, which are licensed commercial products to be obtained directly from Micrium.

For further information on SDK RTOS examples, please see the ADuCM350BBCZ Device Drivers Release Notes and the ADuCM350BBCZ Software Users Guide documents which can be found in the "doc" directory of the SDK.

Q: What version of µC/OS-II is supported?

A:

  • Version: v2.92.08
  • Release Date: 2013-03-26
  • File Name: KRN-KR2XX-PKG000-X-P1.zip

Q: Does the SDK provide support for any other RTOS (e.g. FreeRTOS)?

A: Currently Micrium µC/OS-II is the only RTOS supported by the SDK.

Q: Is a USB stack provided as part of the SDK?

A: While the SDK does provide examples for USB Mass Storage Class (MSC) and Personal Healthcare Device Class (PHDC), the USB stack itself is provided by Micrium. Note that ADI does not deliver the Micrium source files, which are licensed commercial products to be obtained directly from Micrium.

Q: What version of the USB Stack is supported?

A:

     µC/USB-Device Core

  • Version: v4.01.01
  • Release Date: 2012-09-11
  • File Name: USB-USBD-000000-X-P1.zip

     µC/USB-Device MSC

  • Version: v4.01.01
  • Release Date: 2012-09-11
  • File Name: USB-USBD-MSCXXX-X-P1.zip

     µC/USB-Device PHDC

  • Version: v4.01.01
  • Release Date: 2012-09-11
  • File Name: USB-USBD-PHDCXX-X-P1.zip
Tags: rtos iar firmware aducm350 usb_stack sdk toolchain aducm35x software_development_kit ewarm usb embedded_software micrium Show More