Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM350 FAQ SPI
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM350 FAQ SPI

Q:  What is the difference between SPI0/1 and SPIH?

A: Each SPI has identical functionality, though SPIH is capable of higher transfer rates. From an SPI programming and users model perspective, SPIH, SPI0, and SPI1 are identical. The main difference between SPIH and SPI0/SPI1 is the internal bus interface that they are connected to. SPIH is connected to a higher performance advanced peripheral bus (APB), which is always clocked at the higher system clock rate (HCLK) and contains fewer modules requiring arbitration. SPI0 and SPI1 are connected to the main advanced peripheral bus (APB), which selectively can be clocked at a lower rate (PCLK) and whose latency is more uncertain due to a greater number of modules requiring arbitration. This means that under higher data rates, SPIH can move data more efficiently and with lower latency. SPIH is recommended for use with high data rate peripherals.

Q: Are there any restrictions in programming the SPI in DMA mode?

A: All SPI DMA transfers are 16-bit wide and the DMA should be programmed accordingly. For example, if 16 bytes of data are to be transferred over the SPI, the DMA should be programmed to perform eight 16-bit transfers. If 17 bytes are to be transferred, eight 16-bit transfers would be required, the additional byte is discarded. Data errors will occur if the DMA transfers are programmed as byte-wide transfers. This improves DMA efficiency and reduces DMA interrupt overhead. Odd-sized data byte counts in DMA mode cause data buffer overruns.



Q: What is the functionality of TIM bit in the SPI_CONTROL register?

A: The TIM bit defines the mode of transfer initiation (in Master mode) and interrupt generation (in master/slave modes).

      a. It should be set for all cases involving a Tx (either Tx-only or full-duplex).

      b. For transfers involving Rx only, this bit should be cleared.

When TIM=1, SPI starts the transfers with a write to the SPI TX register.

When TIM=0, SPI expects a read of Rx-FIFO to start the dta transfer. And most importantly, this read should happen when a byte transmission is not going on. That is, when there is no SCLK toggling happening over the interface.

Q: I am using SPI1 to transfer data from the ADuCM350 on the Eval-ADUCM350EBZ. The SCLK doesn't look right and data will only transfer successfully at very low data rates. What is the cause of this? Is it an SPI drive strength problem?

A: This is not an SPI drive strength problem. The SPI1 SCLK pin can also be used as an external GPIO. For this reason, a push-button switch (S4) has been implemented on the Eval-ADUCM350EBZ motherboard. This button has an associated de-bounce capacitor (C5) and this cap is affecting the SLI1 SCLK. The solution is to remove 0r resistor R12 from Eval-ADUCM350EBZ, which will isolate the cap and switch.



Q: Is there a minimum high (inactive) time for CS between transfers?


A: Yes. If CS is to go high (inactive) between transfers, it should be high for a minimum of 1 SCLK period.


Tags: spi aducm350 spi0 sclk spi1 spidma spih aducm35x tim Show More