Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.

Introduction

To achieve higher accuracy and repeatability of measured sensor impedance using ADuCM350, the RCAL, RTIA , CTIA and the DAC output voltage during the measurement needs to be optimized.

The accurate results can be produced when the ADuCM350 SNR is higher. To achieve higher SNR, the DAC output needs to be around 600 mVp and the ADC input should be  around 750 mVp.

600 mVp – Maximum allowable swing from DAC output.

750 mVp – Maximum allowable swing at ADC input.

To calculate the RCAL , RTIA and DAC Output code, the below items needs to be identified.

  1. The minimum sensor impedance.
  2. Access resistance and Capacitance.
  3. Mode of operation such as 2-wire,4-wire and 4-wire Bio-Isolated.
  4. Frequency of interest.

Based on the above parameters, the RCAL , RTIA , CTIA and DAC Output code values can be calculated.

Please refer to the application note “AN-1271-Optimizing the ADuCM350 for Impedance Conversion” for detailed explanation of this calculations.

4-wire Measurement Set-up with RACCESS:

The diagram shown below depicts the 4-wire measurement to be performed using ADuCM350 with RACCESS to identify the unknown Z value connected between the AFE channels 6 and 3.

RCAL,RTIA,CTIA and DAC Output Selection Procedure:

For the 4-wire measurement diagram shown above,consider the below parameters.

  1. Minimum Zsensor = 2000 Ω ;
  2. RACCESS1-4 = 10 KΩ;
  3. Frequency of measurement = 50 KHz.
  4. Mode of measurement = 4-Wire with only access resistances.

With the above mentioned inputs,the RCAL,RTIA,CTIA and DAC Output values can be selected.

RCAL Selection  Procedure:

The RCAL resistor value can be selected as same as the minimum Zsensor value. This allows larger signal during calibration and hence the improved accuracy.

RCAL  = Minimum Zsensor = 2000 Ω.

RTIA Selection  Procedure:

The RTIA value can be calculated by following the below steps:

1.Calculate the total impedance across the channels. In our case, between AFE6-3 :

      = RACCESS1 + RACCESS4+ Zsensor

      =10 KΩ + 2000 Ω + 10 KΩ = 22 KΩ.

2.Calculate the current through the channels(AFE6-3) :

  = (Maximum DAC output voltage * Attenuation Factor) / Total impedance across the channels.

  • The Maximum DAC output voltage allowable is 600 mVp.
  • The attenuation factor is the attenuation of RCF incorporated at the DAC. The RCF has a cutoff frequency of 50 KHz and based of the frequency of operation , the signal attenuation varies.

The attenuation factor can be calculated by using the below equation :

1/(SQRT((1+(F/Fc)^2))).

Where as

  • Fc – cutoff frequency of RCF which is 50 KHz.
  • F – DAC output frequency.

Considering our frequency of interest which is 50 KHz,The attenuation factor is 

= 1/(SQRT((1+(50000/50000)^2))) = 0.707

3.The current through channels can be calculated by substituting the above values.

= 600 mVp * 0.707  / 22 KΩ

= 19.28  µA

4.Now, Calculate the optimal RTIA by dividing the maximum allowable ADC input(750 mVp) with the calculated current through the channel.

  = 750 mVp / 19.28 µA = 38.9 KΩ.

5. Atlast,select the closest available standard resistor value

i.e. RTIA  = 39.2 KΩ 1%.

CTIA Selection  Procedure:

The CTIA value can be selected by identifying the cutoff frequency of the measurement signal, RTIA and attenuation factor.

CTIA = 1/(2*∏*Fc* RTIA).

Fc – Cutoff frequency of the RC filter.

The Fc needs to be carefully selected here. If Fc is too close to desired frequency of interest , the ADC input will be attenuated due to the RC filter rolloff.

Considering ,the cutoff frequency ten times the measurement frequency gives a attenuation factor of 0.995.The cutoff frequency selected is 500 KHz.

Now, the CTIA can be calculated by

= 1/(2*∏*500E3*39.2E3)

= ~ 8 pF.

Select the closest available standard capacitor value

i.e. CTIA  = 10 pF 5%.

DAC Output Voltage Selection Procedure:

To calculate the DAC output voltage that needs to be programmed in code, multiply the current through the channel with the sensor impedance.

  = 19.28 µA * 2000 Ω.

  =~39 mV

RCAL,RTIA,CTIA and DAC Output Calculator:

The excel sheet"RTIA_RCAL_CTIA_CALCULATOR.xlsx" attached with this FAQ incorporates the above mentioned procedure and calculates the RCAL,RTIA,CTIA and DAC Output as per measurement inputs.

Signal Swings Across AFE Channels

By using the calculated the RCAL , RTIA , CTIA and DAC Output code values, the DAC output swing captured across the AFE channels 3-6 are shown below :

Please note that the maximum swing across the AFE channels are only 848 mVp-p instead of 1.2 Vp-p. This is due to the 0.707 attenuation factor introduced by the RCF in TX path of ADuCM350.

Also  the DAC output code, we have programmed is ~39 mV only. This larger swing is introduced by the Raccess resistance of 10 K. The 39 mV swing will be present across the sensor impedance of 2K.

Programming a wrong DAC output in code could cause DAC output saturation or reduced SNR thereby affecting the measurement results.

Signal Swings Across ADC (RTIA) Input:

By using the calculated the RCAL , RTIA , CTIA and DAC Output code values, the signal swing captured across the ADC input is shown below :

Please note that the maximum swing across the ADC input is ~1.5 Vp-p. This helps in achieving maximum SNR and thereby producing accurate measurements.

Conclusion :

Thus optimum values for RCAL, RTIA,CTIA and DAC output needs to be selected for obtaining accurate results using ADuCM350.Use the excel sheet calculator attached with this FAQ for selecting them.

Attachments:
RTIA_RCAL_CTIA_CALCULATOR.xlsx
Tags: ctia aducm350 rcal rtia impedance measurement aducm35x Show More