Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents AFE Transmit Stage
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

AFE Transmit Stage

  • How does the ADuCM350 set a voltage on the sensor ?
  • First step is to consider the DAC and it's transfer function.
    • The VDAC Output Range is 0.2V to 1.0V.
  • This signal is then biased and gain up to produce the output voltage from the Excitation Amplifier, VD, which is the voltage seen by the sensor.
  • VD = ( ( VD-0.6V ) X 2 ) + VBIAS
    • VDAC is referenced to the INAMP reference of 0.6V
    • The Excitation/INAMP Loop has a gain of 2.
    • VBIAS: The Common Mode of the System is setup by the +ve terminal of the TIA.
  • This leads to a transmit channel transfer function that looks like:
  • How does the TIA set the Common Mode of the AFE Measurement Loop ?
  • See diagram below as reference.
  • Assume 2-Wire Measurement with P and N tied internally.
    • In 4-Wire, Raccess would be automatically compensated for on D/P/N and T.
  • TIA Sets Common Mode
    • Positive terminal of the TIA is connected to VBIAS.
    • Therefore the negative terminal of TIA forced to VBIAS. This is a Virtual Ground.
  • T = N = VBIAS
    • T and N are shorted internally
  • Excitation Buffer Forces D so that P – N = 0V
    • But N is forced to VBIAS by TIA
    • So Excitation Buffer drives P to = VBIAS
  • Hence D is forced to have a common mode of VBIAS
    • With the DAC at midscale, the Excitation Buffer
      output sits at VBIAS
  • Example Calculation: Sensor needs to see +450mV on Counter and 0V on Working Electrode. i.e +450mV step across Sensor.
  • Goal is to have P – N = +450mV
    • Assume VBIAS = 1.1V.
    • T = 1.1V = Virtual Ground
    • Given that N = T = VBIAS, this implies that the voltage at the P node needs to be 1.55V
  • Signal swing of Excitation Amplifier output is -800mV to +800mV
  • Dividing this range by the resolution of the DAC
    • 1.6V / 2^12 = 390.725µV
    • Therefore each DAC LSB is equivalent to 390.725µV out of the Excitation Amplifier
    • Midscale of the DAC is equivalent to a 0V difference between P and N
    • Midscale DAC code = 2048 = 0x800
  • 450mV / 390.725µV = 1152 = 0x480
  • 1,1V + 450mV =  0x800 + 0X480 = 0xC80
  • Therefore, the DAC code required for a +450mV step on the sensor is 0xC80
Tags: dac transmit channel aducm350 dac aducm350 aducm35x dac