Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI

The following is a short easy guide to get an Impedance measurement plotted on your PC on receipt of the ADuCM350 evaluation kit, the Eval-ADuCM350EBZ.

The EKSP is GUI based PC software coupled with firmware running on the Eval-ADUCM350EBZ evaluation board which allows the user to easily perform analog front end (AFE) measurements, without having to write any embedded software.

This process assumes you have not downloaded new code on to part or erased the EKSP.hex file that has been downloaded to the ADuCM350 by default. Please go to ADuCM350 FAQ Evaluation Kit Software Platform if you need to re-download EKSP.hex file.

Step 1. Download EKSP Labview GUI Software

The EKSP installer can be downloaded from the ADuCM350 Design Resources Downloads.  This installer will install the GUI based PC software.

Step 2. Connect Eval-ADuCM350EBZ board to PC

Once the software is installed, connect the emulator board (not yet connected to the motherboard) to the target PC using the USB cable provided and open Device Manager (can be found in Control Panel) on the PC. Under Ports, the emulator board will be recognized as JLink CDC UART Port (COMX, where X is the COM port number). Take note of the COM port number.

Please ensure the Switch Mux Config Board is mounted correctly on the Eval-ADuCM350EBZ board as shown below.


Step 2. Run EKSP Labview GUI

Launch the ADuCM350 EKSP GUI software. ADuCM350_EKSP.exe can be found in the Start menu under All Programs -> Analog Devices -> ADuCM350 or in the installation directory (if the default installation path is used: C:\Program Files (x86)\Analog Devices\ADuCM350).

The software will automatically detect the available COM ports and connect with the board. If more than one board is detected, the user will have the option of which board to connect to.

If the software fails to connect, try some or all of the following:

  • Ensure that the USB-SWD/UART-EMUZ emulator board is connected to the PC and to the Eval-ADUCM350EBZ motherboard
  • Reset the Eval-ADUCM350EBZ motherboard
  • Check that the links on the Eval-ADUCM350EBZ motherboard are in the correct (default) positions see UG-668 in Design Documentation folder.

Step 3. Quick Impedance Measurement (Frequency Sweep)

Once GUI Opens:

  1. Click Go
  2. Click Plot

By default, the ADuCM350 EKSP software is configured to do a frequency sweep impedance measurement, just by clicking Go. The default values will trigger multiple impedance measurements, each with an AC excitation voltage amplitude of 6.36 mV and frequencies from 1 kHz to 50 kHz in 1 kHz steps.

While the measurements are being performed, the mouse cursor will change to the system busy cursor and the Impedance Measurement Status LED will light. Once the measurements are complete, the LED will extinguish and Measurement Return Data will be populated with results.

To view a simple plot of the results, click the Plot button below the results and a plot will open in a separate window, as shown in Figure 6. Click Plot on both the ADuCM350 EKSP Tab and again on the Plot AFE Results Tab, to plot the values specified in the Plot Selection drop down menu (Impedance Magnitude vs. Frequency by default). Alternative plotting options can be found in the Plot Selection drop down menu. Click Close to close this window.

The default plot below is a Measured Versus Theoretical Impedance Frequency Sweep.

For more information on the EKSP Labview GUI  and how to used it please refer to

ADuCM350 FAQ Evaluation Kit Software Platform which is an FAQ and has a link to the EKSP Userguide.

Tags: aducm350 aducm35x