Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADUCM360/361 ADC input or external reference short/open detection
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • -ADuCM360: FAQ
    • ADuCM360 VDAC interpolation mode
    • ADuCM360, CRC-24 initial values
    • ADUCM360/361: ADC ENOB Calculation
    • The ADI Elves Software Tool
    • ADUCM360/361: Configuring unused ADC inputs
    • ADUCM360/361: Convert ADC reading to voltage
    • ADUCM360/361: Differences between Serial Wire Debug and JTAG
    • ADUCM360/361: Memory-to-Memory DMA transfers
    • ADUCM360/361: Register Information
    • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates
    • ADUCM360/ADUCM361: External Clock
    • How to use ADICUP360 with EmBitz
    • Difference between ADuCM360 and ADuCM361
    • ADUCM360/361 ADC input or external reference short/open detection
    • ADuCM360 - IAR Embedded Workbench
    • ADuCM360 offset voltage
    • ADuCM360 programming in production
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADUCM360/361 ADC input or external reference short/open detection

Q 

Can an open/short on an ADC input or external reference input be detected?  I
want to be  sure that wiring issues can be detected in my application.

 

A 

The ADuCM360/361 provides 2x 50uA diagnostic current sources.  When switched
on, these current sources can be selected to output current on any ADC input.

a.To detect a short:
Enable the current source to connect to one of the inputs.(For example,
ADC1CON[11:10] = [01]) Normally the ADC result should be 50uA*R1. If a short is
present,
the ADC result will be ~0V.

b.To detect an open connection to an ADC input:
Enable the current source to two Analog input pins: (For example,
ADC1CON[11:10] = [11])
Normally, the ADC result should be 50uA*(R1.-R2)
If the ADC result is larger than even the worst case matching of R1 and R2, an
open  connection is detected.

c.An error on the external reference inputs is detected using the DETSTA[4]
status bit.
This bit is set to 1 if the external reference source connected to VRFE+/VREF-
is <= 400mV.
Note, this bit is not valid for the EXTREF2IN+/EXTREF2IN- inputs.

Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More