Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: ADI’s Commercial Space Screening Approach for Agile, High-Reliability Payloads
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADUCM360/361: Convert ADC reading to voltage
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • -ADuCM360: FAQ
    • ADuCM360 VDAC interpolation mode
    • ADuCM360, CRC-24 initial values
    • ADUCM360/361: ADC ENOB Calculation
    • The ADI Elves Software Tool
    • ADUCM360/361: Configuring unused ADC inputs
    • ADUCM360/361: Convert ADC reading to voltage
    • ADUCM360/361: Differences between Serial Wire Debug and JTAG
    • ADUCM360/361: Memory-to-Memory DMA transfers
    • ADUCM360/361: Register Information
    • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates
    • ADUCM360/ADUCM361: External Clock
    • How to use ADICUP360 with EmBitz
    • Difference between ADuCM360 and ADuCM361
    • ADUCM360/361 ADC input or external reference short/open detection
    • ADuCM360 - IAR Embedded Workbench
    • ADuCM360 offset voltage
    • ADuCM360 programming in production
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADUCM360/361: Convert ADC reading to voltage

Q 

Please explain how I convert an ADC reading to a voltage value? Please give an
example for  G=1 and also for G=8.

 

A 

Calculating the voltage from the ADC reading is very simple and requires very
few CPU instructions.
Also, there is no adjustment required for different gain settings - the ADC
hardware handles the  gain adjustment automatically for the user.
The following code example is valid for all gain settings when the internal
1.2V reference is selected as the ADC reference source and when the ADC output 
code is set for 2's complement  mode (ADC1CON.18=1).

         float fVolts, fVoltage = 0.0;
         volatile  long lADC1Result = 0;      // Signed 32-bit integer
fVolts    = (1.2 / 268435456);       // Calculate LSB size= VREF/2^28
fVoltage = (lADC1Result * fVolts);   // Convert ADC result to volts
Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More