Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADUCM360/361: Memory-to-Memory DMA transfers
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • -ADuCM360: FAQ
    • ADuCM360 VDAC interpolation mode
    • ADuCM360, CRC-24 initial values
    • ADUCM360/361: ADC ENOB Calculation
    • The ADI Elves Software Tool
    • ADUCM360/361: Configuring unused ADC inputs
    • ADUCM360/361: Convert ADC reading to voltage
    • ADUCM360/361: Differences between Serial Wire Debug and JTAG
    • ADUCM360/361: Memory-to-Memory DMA transfers
    • ADUCM360/361: Register Information
    • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates
    • ADUCM360/ADUCM361: External Clock
    • How to use ADICUP360 with EmBitz
    • Difference between ADuCM360 and ADuCM361
    • ADUCM360/361 ADC input or external reference short/open detection
    • ADuCM360 - IAR Embedded Workbench
    • ADuCM360 offset voltage
    • ADuCM360 programming in production
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADUCM360/361: Memory-to-Memory DMA transfers

Q 

Are memory-to-memory DMA transfers supported on the ADuCM360, and ADuCM361?

 

A 

Yes, memory-to-memory transfers are supported on ADuCM360 and ADuCM361.

Any of the dedicated DMA channels can be used for this type of transfer i.e.
there is no specific channel for memory-to-memory transfer.  In the example
below, channel 0 (SPI1TX DMA channel) is used.

1)  Flash to SRAM
•Setup the DMA base pointer
  oSource end pointer pointing to a location in Flash
  oDestination end pointer pointing to a location in SRAM
  oAutorequest DMA transfer type
•Enable DMA channel 0
•Enable uDMA
•Initiate a software request on channel 0

2)  SRAM to Flash
Before starting the transfer:
•The Flash destination page must be erase.
•The Flash write must be enabled.

The sequence described in 1) can then be used with source and destination
pointer swapped.
Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More