Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Upcoming Webinar: Simplify High-Accuracy Instrumentation Design with Latest Precision Data Converters

    Join us for an insightful webinar on how ADI’s Precision technology is transforming the landscape of high accuracy instrument design with cutting-edge...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    Exploring DCM and CCM in SMPS: Part 1 of 6

    Power supplies are the unsung heroes of electronic devices, ensuring that they receive the precise, stable, and clean DC voltages they need to function...

     

    Let’s Take a Field-Bus Trip

    Let’s dive deep into what makes field buses unique compared to each other. Building on our previous blog post, What Makes Field Bus Communication Unique...

    Latest Blogs

    • Countable vs Non-countable Faults
    • Power Your Signal: DAS Networks Unleashed: Part 2 of 4
    • Combining Functional Safety and Availability Using Redundancy
    • Top 3 Engineering Blogs That Captivated Minds on EngineerZone
    • How to Generate a Custom Profile for Optimal System Performance
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
Precision Microcontrollers
  • Microcontrollers
Precision Microcontrollers
Documents CN0300: Increasing DAC Resolution
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • More
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • -CN0300: FAQ
    • CN0300: Calibration Options
    • CN0300: DAC output settling time
    • CN0300: Increasing DAC Resolution
    • CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?
    • CN0300: Maximum Loop Voltage (AIN8 connected to INT_Vref)
    • CN0300: Power Consumption
    • CN0300: Type-K or Type-J thermocouple instead of Type-T
    • CN0300: AIN7/Vbias
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

CN0300: Increasing DAC Resolution

Q 

Are there any options for increasing the DAC resolution to greater than
12-bits?

 

A 

Yes. CN0145 for the ADuC7060 shows how a PWM output can be used as a DAC. This
circuit can also be used for the ADuCM360 as it has the same 16-bit PWM.
Another option is to enable the ADuCM360 DAC interpolation mode by setting
DACCON[3]=1.  Note, when using DAC interpolation an external RC filter is
required to generate a smooth DC voltage – again CN0145 should be referred to. 
Note, DAC interpolation mode for the ADuCM360 does not work with DAC NPN mode
so, an external OP-AMP is required.

http://www.analog.com/en/circuits-from-the-lab/CN0145/vc.html
Tags: aduc cortex m3 aducm360