Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • -CN0300: FAQ
    • CN0300: Calibration Options
    • CN0300: DAC output settling time
    • CN0300: Increasing DAC Resolution
    • CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?
    • CN0300: Maximum Loop Voltage (AIN8 connected to INT_Vref)
    • CN0300: Power Consumption
    • CN0300: Type-K or Type-J thermocouple instead of Type-T
    • CN0300: AIN7/Vbias
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?

Q 

For CN0300, could the ADuCM361 be used – in other words implement the
temperature readings and DAC feedback control with just one ADC instead of 2?

 

A 

As the circuit is currently built, if one ADC is used for everything, the DAC
output voltage is not stable. The instability occurs when AIN9 is
enabled/disabled as the ADC input channel. When this change occurs, the input
impedance on AIN9 changes due to switches on the input MUX being turned off/on.

When AIN9 is always selected as the input to AIN0 as is the case for this
ADuCM360 implementation, this is not an issue.
Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More