Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

     

    TIA Me Up, But Keep It Stable: Part 2 of 3

    Imagine trying to measure a current so tiny that it’s almost invisible. How is that even possible? How do we even convert that current signal into something...

    Latest Blogs

    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
    • Achieving Power Over Data with RS-485 Transceivers
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents CN0300: DAC output settling time
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • -CN0300: FAQ
    • CN0300: Calibration Options
    • CN0300: DAC output settling time
    • CN0300: Increasing DAC Resolution
    • CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?
    • CN0300: Maximum Loop Voltage (AIN8 connected to INT_Vref)
    • CN0300: Power Consumption
    • CN0300: Type-K or Type-J thermocouple instead of Type-T
    • CN0300: AIN7/Vbias
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

CN0300: DAC output settling time

Q 

After a reset sequence, how long does it take for the DAC output to settle?  I
assume a number of ADC readings are required?

 

A 

There is a settling period required which will take several seconds after a
reset sequence. For the first write to the DAC output, the function “UpdateDAC
()” is called – this function does not use DAC calibration values and it does
not use ADC compensation. After this, the function “FineTuneDAC()” is used to
update the DAC and this uses the ADC feedback value.  Applications should allow
for a number of iterations of this loop taking several seconds to see a settled
output current. The debug strings sent to the UART list by how many DAC codes
the DAC is tweaked with every pass of “FineTuneDAC().”
Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More