Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Join us for an in-depth webinar where we dive into the world of EMC testing applied to ADI’s digital isolators. We''ll walk through the test setups, standards...
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
      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    By Christopher Nunes What happens when your system needs to talk across noisy or high-voltage boundaries? Isolation steps in. In a previous blog post...

     

    Understanding Safe Failure Fraction: Can There Be Multiple Values?

    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...
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
Precision Microcontrollers
  • Microcontrollers
Precision Microcontrollers
Documents CN0300: Calibration Options
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • -CN0300: FAQ
    • CN0300: Calibration Options
    • CN0300: DAC output settling time
    • CN0300: Increasing DAC Resolution
    • CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?
    • CN0300: Maximum Loop Voltage (AIN8 connected to INT_Vref)
    • CN0300: Power Consumption
    • CN0300: Type-K or Type-J thermocouple instead of Type-T
    • CN0300: AIN7/Vbias
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

CN0300: Calibration Options

Q 

Can you explain the calibration options in the example code?

 

A 

Two #defines in the “Thermocouple_to_DAC.c” configure the calibration settings
for the ADC  and the DAC.

For the ADC:
#define calibrateADC1 0 // Set to 0 if you don't want to calibrate
     // Set to 1 if you want to calibrate externally and save to flash
    // set to 2 if you want to load previously saved values from flash
By default, a value of 0 is used

For the DAC:
#define calibrateDAC  1 // Set to 0 if you don't want to calibrate and just use
default values
   // Set to 1 if you want to calibrate externally and save to flash
   // set to 2 if you want to load previously saved values from flash
By default, a value of 1 is used.

To use any calibration mode, you must have the UART connected to a PC – use the
SWD-UART interface board to connect to a USB port of your PC – see the CN0300
document for more details.
Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More