Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM360 programming in production
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • -ADuCM360: FAQ
    • ADuCM360 VDAC interpolation mode
    • ADuCM360, CRC-24 initial values
    • ADUCM360/361: ADC ENOB Calculation
    • The ADI Elves Software Tool
    • ADUCM360/361: Configuring unused ADC inputs
    • ADUCM360/361: Convert ADC reading to voltage
    • ADUCM360/361: Differences between Serial Wire Debug and JTAG
    • ADUCM360/361: Memory-to-Memory DMA transfers
    • ADUCM360/361: Register Information
    • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates
    • ADUCM360/ADUCM361: External Clock
    • How to use ADICUP360 with EmBitz
    • Difference between ADuCM360 and ADuCM361
    • ADUCM360/361 ADC input or external reference short/open detection
    • ADuCM360 - IAR Embedded Workbench
    • ADuCM360 offset voltage
    • ADuCM360 programming in production
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM360 programming in production

Q 

We tried to use CM3WSD for production downloading (hex file via CM3WSD
application) but I don’t have physically access to the P2.2 which is used for
setting the chip in serial download mode.

A possible solution would be to have the production use the IAR IDE to download
the code via the SWDP. I’m just afraid that our production will change the code
by accident and download a changed code. It’s easier for them if they just
download a hex file which they cannot change.

Do you know if Analog Devices (or anyone else) have a desktop SW which can
download the hex file via SWDP?

 

A 

IAR seems to be able to just download the out file generated by the compiler
(Project>Download>download file).
The out file should be IAR's version of a hex file. So you could just have an
empty project and just download the out file using that project so the out file
won't be modified.

Alternatively Keil uVision can download hex files.
http://www.keil.com/support/man/docs/uv3/uv3_fl_hexdownload.htm
The free version of uVision should be able to do it.

There's a paid for utility from Segger called J-Flash.

Finally for another free way it's also possible for IAR to generate a binary
file. The binary file can be programmed by j-link commander.
The commands needed are :

device aducm360
erase
loadbin filename.bin 0

Tags: aduc cortex m3 aducm360
  • Share
  • History
  • More