Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Join us for an in-depth webinar where we dive into the world of EMC testing applied to ADI’s digital isolators. We''ll walk through the test setups, standards...
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
      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    By Christopher Nunes What happens when your system needs to talk across noisy or high-voltage boundaries? Isolation steps in. In a previous blog post...

     

    Understanding Safe Failure Fraction: Can There Be Multiple Values?

    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...
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
Precision Microcontrollers
  • Microcontrollers
Precision Microcontrollers
Documents Continuously Amperometric Measurement Example
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • -Continuously Amperometric Measurement: FAQ
    • Continuously Amperometric Measurement Example
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Continuously Amperometric Measurement Example

System Setup(All settings are similar to Amperometric Measurement Example)

  • Documentation:
    • AN-1281
  • Hardware
    • Eval-ADuCM350EBZ
    • ADuCM350 Switch Mux Config
  • Software
    • AmperometricMeasurement example in IAR Embedded Workbench, attached source file is used to replace original AmperometricMeasurement.c
  • View data in Comms port

Software Configuration for generating trapezoid.

Modify the parameters as you want, please note that SLOPE1 time in second is (SLOPE1/320000). In this case, we set SLOPE to 320000 means slope time is 1s.

RCAL is 1kOhm on Switch Mux Config Board and RTIA is 5kOhm.

Measurement Results.

By default, this program will generate trapezoid waveform between AFE4 and AFE6(Mux configuration: D-AFE4, P-AFE4, N-AFE6, T-AFE6). Using oscilloscope to monitor voltage on AFE4 we got following picture. Voltage on AFE6 is 1.1V constant, so the DC_LEVEL1 is 1.1V-1.1V = 0, same as we defined.

Using PuTTY to observe UART(BaudRate: 115200bps) output and draw the curve in excel.

Attachments:
ContinuousAmperometricMeasurement.c.zip
Tags: amperometric aducm350 trapezoid generator aducm35x continuous
  • Share
  • History
  • More