Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents How to use ADICUP360 with EmBitz
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • -ADuCM360: FAQ
    • ADuCM360 VDAC interpolation mode
    • ADuCM360, CRC-24 initial values
    • ADUCM360/361: ADC ENOB Calculation
    • The ADI Elves Software Tool
    • ADUCM360/361: Configuring unused ADC inputs
    • ADUCM360/361: Convert ADC reading to voltage
    • ADUCM360/361: Differences between Serial Wire Debug and JTAG
    • ADUCM360/361: Memory-to-Memory DMA transfers
    • ADUCM360/361: Register Information
    • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates
    • ADUCM360/ADUCM361: External Clock
    • How to use ADICUP360 with EmBitz
    • Difference between ADuCM360 and ADuCM361
    • ADUCM360/361 ADC input or external reference short/open detection
    • ADuCM360 - IAR Embedded Workbench
    • ADuCM360 offset voltage
    • ADuCM360 programming in production
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

How to use ADICUP360 with EmBitz

After I didn't get the functionality out of the box with the provided tool-chain - I missed to reset/restart the debugging without leaving the Debug-Mode and that I wasn't able to suspend/pause the project, I looked around for a quick solution to get this functionality with the ADICUP360 to get my project debugged.

I found EmBitz which is based on Code::Blocks (like emIDE) and was very fast able to set it up to be used with the ADICUP360.

For everyone who want to check that out as well - here below a short How-to

1. download EmBitz from https://www.embitz.org/ - unzip and install

2. download mbed serial driver and install from - https://os.mbed.com/handbook/Windows-serial-configuration

3. download the attached openocd.zip - unzip to c:\openocd

4. connect the ADICUP360 to your PC and run the batch "startADICUP360OpenOCDserver.bat", allow access & close the Command Window

5. download the attached example and unzip anywhere you want

6. Start EmBitz and "Open a existing project" - select the example project "emBitz_ADuCM360_Blink.ebp"

7. Build the Project and Start Debug - the project will be loaded to Flash and stops at the entry of the main() function

The attached project has all configuration set for the given installation and can be used as base for your own projects.

Attachments:
ez.analog.com/.../ADuCM360_5F00_Blink.zip
ez.analog.com/.../openocd.zip
Tags: adicup360 embitz aducm360