Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Does the MAX32664 use SPI?
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • -MAX32664GWEA+: FAQ
    • Can the MAX32664A algorithm compensate for future sensor degradation or smartphone “aging”?
    • Does the MAX32664 provide the raw sensor data, in addition to the processed sensor data?
    • Does the MAX32664 support field updates?
    • Does the MAX32664 use SPI?
    • I am observing unexpected results when pulling data from a smart sensor FIFO at high rates. What is going on?
    • Is the KX-122 accelerometer in the MAXREFDES101 configured to 2g, 4g or 8g range?
    • Is there an EV Kit for the MAX32664?
    • Is version A of the MAX32664 Sensor Hub storing data into the FIFO at 100Hz or sampling the sensors at 100Hz?
    • MAX32664 Solder ball material?
    • The MAX32664GWEA, B, C, D does not go to application mode when using the RST_N and MFIO lines. The device mode returns bootloader mode even after waiting 1 sec. What might be wrong?
    • What is the difference between the MAX32664A and the MAX32664B?
    • What is the MAX32664?
    • What is the MAX32664A?
    • What is the MAX32664B?
    • Which accelerometer is on the MAXREFDES220?
    • Which biometric parameters does the MAX32664 (A) measure?
    • Which optical sensors can be used with the MAX32664 (A)?
    • Which optical sensors can be used with the MAX32664 (B)?
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Does the MAX32664 use SPI?

Revision Creation Date Revision Author
Current Revision 11 Feb 2026 12:47 AM EngineerZone
Revision #6 10 Feb 2026 1:54 PM MSDAPI
Revision #5 10 Feb 2026 1:54 PM MSDAPI
Revision #4 19 Dec 2023 2:53 PM MSDAPI
Revision #3 19 Dec 2023 10:52 AM MSDAPI
Revision #2 6 Dec 2023 12:44 PM MSDAPI
Revision #1 20 Jun 2018 3:17 AM MSDAPI
  • Compare Versions View current version