Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Is there an EV Kit for the MAX32664?
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • -MAX32664GWEA+: FAQ
    • Can the MAX32664A algorithm compensate for future sensor degradation or smartphone “aging”?
    • Does the MAX32664 provide the raw sensor data, in addition to the processed sensor data?
    • Does the MAX32664 support field updates?
    • Does the MAX32664 use SPI?
    • I am observing unexpected results when pulling data from a smart sensor FIFO at high rates. What is going on?
    • Is the KX-122 accelerometer in the MAXREFDES101 configured to 2g, 4g or 8g range?
    • Is there an EV Kit for the MAX32664?
    • Is version A of the MAX32664 Sensor Hub storing data into the FIFO at 100Hz or sampling the sensors at 100Hz?
    • MAX32664 Solder ball material?
    • The MAX32664GWEA, B, C, D does not go to application mode when using the RST_N and MFIO lines. The device mode returns bootloader mode even after waiting 1 sec. What might be wrong?
    • What is the difference between the MAX32664A and the MAX32664B?
    • What is the MAX32664?
    • What is the MAX32664A?
    • What is the MAX32664B?
    • Which accelerometer is on the MAXREFDES220?
    • Which biometric parameters does the MAX32664 (A) measure?
    • Which optical sensors can be used with the MAX32664 (A)?
    • Which optical sensors can be used with the MAX32664 (B)?
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Is there an EV Kit for the MAX32664?

Revision Creation Date Revision Author
Current Revision 19 Dec 2023 2:53 PM MSDAPI
Revision #3 19 Dec 2023 10:52 AM MSDAPI
Revision #2 6 Dec 2023 12:44 PM MSDAPI
Revision #1 20 Jun 2018 3:04 AM MSDAPI
  • Compare Versions View current version