Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents ADuCM350 SDK v2.3.0.0 now available
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

ADuCM350 SDK v2.3.0.0 now available

The latest version of the ADuCM350 Software Development Kit, v2.3.0.0, is now available to download. The download is available here (registration required). The changes in SDK v2.3.0.0 are as follows (as per the ADuCM350BBCZ Device Drivers Release Notes):

Maintenance release, including fixes/features:

  • USB/RTOS
    • Added support for the USB Communications Device Class (CDC) with accompanying example.
    • Updated support for Micrium’s latest uC/OS-II release (4.04.01).
    • Updated to the latest USB driver from ADI, featuring the following improvements:
      • USB host and device modes are integrated
      • DMA mode 1 is fully functional
      • Improved throughput
    • Removed obsolete bsp directory and files and revised examples to build without them.
  • Removed deprecated dynamic GPIO pin multiplexing APIs from the GPIO service.  A static pin multiplexing GUI is now used to reduce target code footprint and code complexity.  (See “Static Pin Multiplexing” in “ADuCM350BBCZ Software Users Guide” for details.)
  • Removed “TEST_COMMON_USES_UART” STDIO redirection macro.  Any UART output must be be managed at the application level -- after first configuring the UART pins as required as part of static pin mux configuration process (See “PinMuxUI” in the “tools” directory of this release).  UART output has been added at application level for Analog Front End (AFE) based examples to facilitate returning results from the ADC.
  • SPI Device Driver
    • Added support for designating any GPIO pin for use as SPI chip select.
    • Added DMA data chunking to schedule large data transactions into a chain of smaller DMA descriptor blocks, as needed.  The DMA “ping-pong” cycle type is used to automatically switch/update descriptors.  This is entirely within the SPI driver and transparent to the user.
    • Enforced DMA mode size checking of the “DataSize” member in the ADI_SPI_TRANSCEIVE_TYPE structure (used by both adi_SPI_MasterTransfer() and adi_SPI_SlaveTransfer() APIs) to insure evenly-size counts and buffer allocations for DMA transactions.  The 8-bit byte count must be evenly-sized because underlying SPI controller employs only 16-bit DMA mode.
    • Added DMA error handlers to the SPI examples to intercept “invalid” DMA descriptor interrupts resulting from the intentional use of invalid DMA cycle type to mark the end of a multiple DMA descriptor chain.  Such errors are allowed by the handler while other DMA errors are trapped (bus errors, etc.)
  • Examples removed:
    • SpiMasterSlaveTest example removed. If this example is required, please contact ADI. See Support section.
    • Mipi_SSD1963_Test example removed due to hardware supply issue.