Post Go back to editing

Not able to program ADICUP3029, nor able to erase using serial flash utility

Category: Software
Product Number: ADuCM3029

I am trying to program ADICUP3029 board. After converting the MAINTAINACE drive to DAP link drive, I could program once using the example blinky project.
While debugging I think I pressed the boot or reset button (I dont remember which). After this I am not able to program the board nor able to use serial utility to erase the board. Following are the error logs I am getting.

Both Power and UART switches are kept in USB position.

Cross core debug log - debug configuration (Board - Analog Devices ADuCM3029(DFP), Interface - CMSIS-DAP, Max speed 1MHz, Reset option - System Reset)

Open On-Chip Debugger (Analog Devices 0.12.0-1.3.3) OpenOCD 0.12.0 (2026-05-26-15:18)
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
0
cortex_m reset_config sysresetreq
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: FW Version = 1.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 0 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 1000 kHz
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Examination failed
Warn : target aducm3029.cpu examination failed
Info : [aducm3029.cpu] starting gdb server on 3333
Info : Listening on port 3333 for gdb connections
memory bus access delay set to 6 tck
adapter speed: 1000 kHz
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Debug AP not available, reset NOT asserted!
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Debug AP not available, reset NOT asserted!
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Debug AP not available, reset NOT asserted!
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Debug AP not available, reset NOT asserted!
Info : SWD DPIDR 0x2ba01477
Error: [aducm3029.cpu] Could not find MEM-AP to control the core
Error: [aducm3029.cpu] Debug AP not available, reset NOT asserted!
Info : SWD DPIDR 0x2ba01477
Error: Target not examined yet
Error: [aducm3029.cpu] Execution of event gdb-attach failed:

Error: Target not examined yet
Error: Target not examined yet
Error: not an Analog Devices Cortex-M based part
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected

Serial flash utility log - (ADuCM302x and 9600 to 115200 baud rate)

Sending second stage kernel.
Read Intel HEX application image with 668 bytes.
No autobaud response.

Please help. I want to be able to use the Cross core IDE again.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.