I am unable to connect to the 'EVAL-ADuCM410QSP1Z' through 'J-Link', so I cannot flash or debug the device. The debugger detects the board and target voltage, but it does not attach to the core. The same behaviour occurs with both my current firmware project and a previously known-good ADuCM410 example.
Setup / steps to reproduce:
1. Connect the 'EVAL-ADuCM410QSP1Z' to a PC over USB.
2. Open 'Keil uVision', 'J-Link Commander', or 'J-Flash Lite'.
3. Select device 'ADUCM410' and interface 'SWD'.
4. Attempt to connect, flash, or start a debug session.
Observed result:
- The debugger detects the 'SW-DP' and target voltage at about '3.3 V'.
- It then fails to attach to the core.
- Reported errors include:
- 'Could not find core in Coresight setup'
- 'Failed to power up DAP'
- Flashing and debugging are not possible.
Additional detail:
I also tried a previously known-good ADuCM410 example project, and the same issue occurs.
Question:
Is there a recommended recovery or mass-erase procedure for the 'EVAL-ADuCM410QSP1Z' in this situation?