Post Go back to editing

UART TX DATA

Thread Summary

The user is troubleshooting a lack of UART activity on the MAX78002EVKit using the example code. The final answer explains that the example code is set up for a loopback test between UART1 and UART2, and no activity will be seen on the TX or RX lines of UART1 if only connected to a logic analyzer or PC. The solution is to modify the code to use a single UART instance for PC communication and remove the loopback configuration.
AI Generated Content
Category: Hardware
Product Number: MAX78002

Hi, I'm trying to establish a UART communication on the MAX78002EVkit. i'm using the example code from analog devices themself for reference. While trying to implement a async message reading implementation i ran into a problem. I'm using a Saleae to log the activity over the tx and rx line. When running the code however no activity is seen on the logger. Im using BAUD rate of 115200 and 8-1bit with no parity. I managed to read data coming in on the RX line before when running my own code but when using the example code the TX line is now showing up and even the RX line stays dead now, even while the com port acknowledges the transaction.

I find it very weird that even the example code does not deliver results. I have everything wired up correctly as stated in the readme file. I hope someone will be able to give me a clue on this matter.

Kind regards!

Parents
  • Hi RMorais,

    The provided example code for the MAX78002EVKit demonstrates a UART loopback test between UART1 and UART2, where:

    • UART1 is configured to receive data asynchronously.
    • UART2 is configured to transmit data synchronously.
    • The example assumes a physical connection between UART1 and UART2:

        P0.12 (UART1_RX) <==> P1.1 (UART2_TX)
        P0.13 (UART1_TX) <==> P1.0 (UART2_RX)

    If you are monitoring the UART lines using a logic analyzer or interfacing with a PC via UART, and you only connect to UART1, you will not observe any activity. This is because the code transmits data through UART2, not UART1.

    In other words, if UART2 is not connected to the logic analyzer or PC, no TX activity will be visible. Additionally, UART1 RX will remain idle unless data is looped back from UART2 or received from an external source. The COM port acknowledgment you observed indicates that the UART peripheral is initialized but not necessarily transmitting any data on the UART1 lines.

    To sum up: No activity is visible on the TX or RX lines connected only to one UART interface, and the Saleae logic analyzer will not capture any traffic if it is attached solely to UART1 or to the PC‑connected port. Although the COM port may appear active on the host computer, the example does not send data to the PC; it only verifies data transfer internally between the two UART modules.

    For PC Communication: If the objective is to send or receive data directly between the evaluation kit and a PC, the example code must be modified. Specifically, only one UART instance (e.g., UART1) should be initialized and used with printf() or MXC_UART_Write() to transmit data to the PC‑connected UART interface. The loopback configuration involving UART2 should be removed in that case.

    Kind regards,

    Haluk

Reply
  • Hi RMorais,

    The provided example code for the MAX78002EVKit demonstrates a UART loopback test between UART1 and UART2, where:

    • UART1 is configured to receive data asynchronously.
    • UART2 is configured to transmit data synchronously.
    • The example assumes a physical connection between UART1 and UART2:

        P0.12 (UART1_RX) <==> P1.1 (UART2_TX)
        P0.13 (UART1_TX) <==> P1.0 (UART2_RX)

    If you are monitoring the UART lines using a logic analyzer or interfacing with a PC via UART, and you only connect to UART1, you will not observe any activity. This is because the code transmits data through UART2, not UART1.

    In other words, if UART2 is not connected to the logic analyzer or PC, no TX activity will be visible. Additionally, UART1 RX will remain idle unless data is looped back from UART2 or received from an external source. The COM port acknowledgment you observed indicates that the UART peripheral is initialized but not necessarily transmitting any data on the UART1 lines.

    To sum up: No activity is visible on the TX or RX lines connected only to one UART interface, and the Saleae logic analyzer will not capture any traffic if it is attached solely to UART1 or to the PC‑connected port. Although the COM port may appear active on the host computer, the example does not send data to the PC; it only verifies data transfer internally between the two UART modules.

    For PC Communication: If the objective is to send or receive data directly between the evaluation kit and a PC, the example code must be modified. Specifically, only one UART instance (e.g., UART1) should be initialized and used with printf() or MXC_UART_Write() to transmit data to the PC‑connected UART interface. The loopback configuration involving UART2 should be removed in that case.

    Kind regards,

    Haluk

Children
No Data