Post Go back to editing

enable debug and mbed reset problems with CCE3.0.3 and win11

Category: Software
Product Number: EVAL-ADICUP360
Software Version: CCE3.0.3

Hi, 

We are test one developer kit.  The code from git and code from CMISIS pack exmaple Blinky can be build successfully. 

When to enable the debugger with GDB OpenOCD,  I only saw interface "CMSIS-DAP".   

Run with debug mode,  the CCE always say about the adapter speed setting.  There no extra options in the CCE3.0.3.  

The latest WIKI was approved by Alexander Goldstein.  I saw it is CCE2.7.0.   The name of CMSIS-DAP is not the same.  

Q1: any way to download CCE2.7.0? 

Q2: could one ADI engineer test the CCE3.0.3 with the same process on the official WIKI and Win11.

Q3: I have the MBED reseting problem as well. I stopped the storage service, no difference.  Can see USB items created OK.  But the file browser keep reset after minute period. 

[Jamper S1 toS4 all as ON, in default mode when the board unpacked]  USB on P14

%%%%%%%%%%%%%%%%  

Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0)  OpenOCD 0.12.0 (2025-04-03-09:09)
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
0
Info : only one transport option; autoselecting 'jtag'
adapter speed: 5000 kHz
DEPRECATED! use 'adapter speed' not 'adapter_khz'
C:/analog/cces/303/ARM/packs/AnalogDevices/ADuCM36x_DFP/1.0.4/openocd/scripts/target/aducm36x.cfg:38: Error: target requires -dap parameter instead of -chain-position!
in procedure 'script' 
at file "embedded:startup.tcl", line 28
at file "C:/analog/cces/303/ARM/packs/AnalogDevices/ADuCM36x_DFP/1.0.4/openocd/scripts/target/aducm36x.cfg", line 38

%%%%%%%%%%%%%%%%%

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.