Post Go back to editing

ADuCM355 external RTIA connection.

Category: Datasheet/Specs
Product Number: ADUCM355

Hi Team,

I'm planning to use the ADuCM355 and perform measurements using the 4-wire impedance method.
My electrode configuration will be:

  • CE0 for HSDAC output

  • AIN1 for HSTIA input

  • AIN2 and AIN3 for voltage measurement

When using the internal RTIA, I just need to close the T2 switch (AIN1) and T9 switch, while keeping T10 and T11 open.

However, if I use an external RTIA, I understand that I need to use AIN1 and DE0 as part of the HSTIA feedback loop.
So, as far as I understand:

  • Close T2 and T9 switches, and set HSRTIACON[3:0] = 0xF (to disable internal RTIA).

  • Connect the external RTIA between AIN1 and DE0.

  • To complete the feedback loop, set DE0RESCON = 0x97, which shorts both Rload3 and RTIA2_03.

  • Then, the feedback loop should be formed as expected.



However, in the ADuCM355 Hardware Reference Manual, it states to close T1 (AIN0) and T10 switches, which results in a different feedback path.

I’m confused about why the T10 switch needs to be closed in that configuration.


Could you please clarify this point?

I would greatly appreciate your help with this final question.

Best regards,

Anzinc.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.