Post Go back to editing

End of life ADUCM355

Thread Summary

The user is experiencing issues compiling ADuCM355 examples with Keil µVision's Arm Compiler 6, as the examples are designed for Arm Compiler 5. The free version of Keil now uses Arm Compiler 6, while Arm Compiler 5 is only available with a licensed MDK-Professional edition. AD suggests using the free version of IAR Embedded Workbench to compile the examples, as they remain compatible.
AI Generated Content
Category: Hardware
Product Number: ADUCM355

I believe this product is nearing it end of life because there is no support from AD regarding the exemples and libraries.

They are supposed to work with ArmCompiler 5 and MDK 5 as recommended in the devkit guide but it is a nightmare to make it work becaus the Keil µVision is now with Compiler 6.

The exemples do not compile with Compiler  6 and not update is provided by AD.

Abandonware ? 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.