Post Go back to editing

Firmware update failure on the ADUCM3029 MCU using Analog Devices - SensorPal interface

Category: Software
Product Number: ADuCM3029
Software Version: Analog Devices - SensorPal version 2.5.3.1
Hello to everyone,
 
I wanted to test the EVAL-ADICUP3029 evaluation board for research purposes using the Analog Devices - Sensor Pal interface, but I am encountering problems updating the firmware on the MCU due to the following failure: ‘The interface firmware FAILED to reset/halt the target MCU’. I have tried different options detailed in the EVAL-ADICUP3029 User Guide, but the problem persists. Here is a brief description of the considerations I have taken into account:
  • Firstly, I have checked that switches S2 and S5 are in the correct positions, i.e., S2 in the USB position and S5 in Wall/USB, as I am powering the board by connecting the cable micro-USB to USB to the laptop.

Secondly, I have tried to program the ADuCM3029 MCU by following the steps below:

1. I dragged and dropped the file 'adi_mbed_interface.hex' into the mass storage device, named 'DAPLINK'. Then two text files were generated ('ASSERT.txt' and 'FAIL.TXT'). In the 'FAIL.TXT' it appears the following text message: 'An internal error has occurred'.

2. I also tried to erase the flash by using the software CrossCore Serial Flash Programmer, but this option didn't work, as it can observe in the screenshot that I show below:



To do the previous step I powered cycle the ADICUP3029 board while holding down the boot switch (S3). The USB was selected on switch S2. I tried different baud rates, but the same problem persisted.

  • Finally, I tried to put the device in 'Maintenance mode' and dragged and copied the file 'ADICUP3029_maintenance_drive_revC_1_0.hex' into the flash. After that, the mass storage device changes its name to "DAPLINK". I procceded to unplug and plug the board to the computer, and repeated the step 2 described above, but the same failure occurs, i.e., "The interface firmware FAILED to reset/halt the target MCU".
Please, could anyone tell me how I can proceed to solve this problem? The board was working properly a week ago. I have tried to use this board in other compueters, but the problem persist.
 
Thank you very much for your attention.
 
Best regards.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.