Post Go back to editing

Calculating Capacitor Series Resistance Using AD5941.

Category: Datasheet/Specs
Product Number: AD5941

I hope you're doing well.

I am currently working on a project involving the AD5941 chip and I need some clarification on how to calculate the capacitor series resistance using the AD5941 chip.

According to the datasheet, the DFTREAL register corresponds to the RALE value. However, based on my experimental observations, it does not seem that DFTREAL directly represents the capacitor series resistance value. I would appreciate it if you could explain the correct formula or method to convert the DFTREAL register value to the series resistance of the capacitor.



Hardware settings:

The measurement was performed using the following pins:

  • RE and SE on one side.
  • CE on the other side.


Software settings:

For the programming part, I am using the Impedance.c library which can be found here:

https://github.com/analogdevicesinc/ad5940-examples/blob/master/examples/AD5940_Impedance/Impedance.c

RCAL: 200.7Ω

RTIA: 5k

SweepStart = 100kHz

SweepStop = 100kHz

Test

Capacitor Value

Capacitor Series Resistance Value

Rz_real

1nf

20/98Ω

11913

4/7nf

4/448Ω

51760

6/8nf

3/364Ω

58746

8/2nf

2/707Ω

63804

10nf

2/383Ω

67674

I would be grateful for any insights or guidance you can share on this topic.

Looking forward to your response.

Best regards.

Daniel Taylor.

Thread Notes

Parents
  • Hi,

    RE and CE must be on one side and SE on other side of the cap.

    Sweepstart and sweepstop are same in your code. Do you not want frequency sweep? If so, you may just disable sweep.

    .SweepCfg.SweepEn = bFALSE.

    However for cap measurement sweep will be required.

    DFTReal is the resistive part of the impedance shown in 2's complement format.

Reply
  • Hi,

    RE and CE must be on one side and SE on other side of the cap.

    Sweepstart and sweepstop are same in your code. Do you not want frequency sweep? If so, you may just disable sweep.

    .SweepCfg.SweepEn = bFALSE.

    However for cap measurement sweep will be required.

    DFTReal is the resistive part of the impedance shown in 2's complement format.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.