| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 0 hours |
Open | |
MAX86178
Production
The MAX86178 is a highly integrated, multiple vital-sign monitoring device with a complete photoplethysmogram (PPG), electrocardiogram (ECG) and biopotential...
Datasheet
MAX86178 on Analog.com
MAX86176
Production
The MAX86176 is a complete photoplethysmogram (PPG) and electrocardiogram (ECG) analog front-end (AFE) solution for wearable applications. The MAX30005...
Datasheet
MAX86176 on Analog.com
MAX32674C
Not Recommended for New Designs
The MAX32674C is an algorithm/sensor hub with embedded software and world-class algorithms for the fitness and medical wearables market meant to interface...
Datasheet
MAX32674C on Analog.com
MAX32663A
Production
The MAX32663A is a low-power sensor hub with embedded firmware and HeartKey® ECG algorithms from B-Secur for wearable and medical devices. It enables...
Datasheet
MAX32663A on Analog.com
Good day, Praise the Lord,
We are a startup in healthcare wearables. We are in a protyping stage. We need a design guide.
Shall I interface MAX32674C with MAX86178 AFE instead of MAX86176. If I am not wrong the only difference is MAX86178 has Bio impedance (EDA) feature. But MAX86176 does not. so Shall I interface MAX86178 with MAX32674C. And also For ECG, we are going to use MAX32663A ECG algorithm hub as MAX32674C does not support ECG. The EDA data from MAX86178 will be processed by Host microcontroller nRF5340 mcu. will it work?
Kindly help with this. Also We have got the full datasheets through NDA process.
Thank you.
Hi JayeshMD, Thank you for your inquiry. A Non-Disclosure Agreement covers the product you are seeking support on, and we are unable to provide support for it in the public EngineerZone community. Per the Analog Devices EngineerZone Code of Conduct, we do not discuss NDA products on EngineerZone. To receive support on this product, please contact the CIC team.