Category: Hardware
Hi Folks,
There seems to be a lack of microcontrollers that have large RAM capacity and high voltage analog inputs. I am looking for a microcontroller that has specs including the following:
- 16 channel or more, 16 bit or greater ADC(s) with a bipolar input of +/-10V or more at a per channel sample rate of >1200 S/s.
- Optional VGA - prefer both gain and attenuation capability in the VGA.
- 32 bit microcontroller with 512kByte or more of data RAM and 512kByte or more of flash memory in the microcontroller.
- 100Mbits/s Ethernet communications or very fast SPI >10Mbits/s
- 20 or more DIO bits.
- Would like to be able to run RTOS or similar low weight real-time operating system.
- A built-in real time clock calendar is highly desirable.
This is an industrial application; not low power. It is the combination of these things that I am looking for. Of course I can build a system using discrete components that can meet the need, but an integrated product would greatly simplify the hardware implementation of such a system.
Is there an integrated microcontroller product out there that can meet the above requirements?
Thanks,
Allan