Post Go back to editing

AD5413 on the same line as a switching output

Category: Hardware

Hello everyone,

we have an application where we need to use a single line as either a digital output or an analog output. The digital output has a voltage range of 10V to 30V (+Ub) and the used AD5413 has a supply of 12V. We need that seperate 12V supply for the AD5413 because of the needed Headroom for the 0-10V interface. Since the absolut maximum ratings only allows AVDD1 + 0.3 V at the VIOut-Pin we have some trouble with the digital output and the internal protective circuit responds, resulting in a short circuit on the digital output. Therefore we used two diodes at the AD5413 supply as shown.

Is there any reason against this approach?

I know the ADG5401F but unfortunately this device is too expensive for this price sensitive project.

Thanks a lot.

Thread Notes