Hello,
I would like to use the MAX32625PICO board to program some custom boards I made featuring a MAX32660 onboard.
As far as I understand, the firmware that comes preinstalled on the PICO lets you use it as a programmer through the SWD connector. I know there are a number of firmware images available on github, I wanted to know if there is a specific one for DIP-pin use at 3.3V.
At the moment I have only been able to successfully program the target through the MAX32625PICO DIP-pins by installing the "max32625_max32660evsys_if_crc_dip_v1.0.3.bin" firmware and powering the target at 1.8V.
Thanks for the help!
Marco
Edit Notes
Made title more precise[edited by: marcop93 at 9:35 PM (GMT -4) on 3 Apr 2024]