Post Go back to editing

max78000 logic level.

Thread Summary

The user inquires about configuring the MAX78000 to support 3.3V logic level for SPI communication when VDDIOH is 3.3V and VDDIO is 1.8V. The final answer directs the user to visit the Analog Devices technical support pages for further assistance. No specific configuration details are provided.
AI Generated Content
Category: Hardware
Product Number: MAX78000

Can MAX78000 configure USART and SPI choose logic level between VDDIO and VDDIOH ?
In our board VDDIOH = 3.3V , VDDIO = 1.8V
Now we use SPI, base on example code the logic level is 1.8V , but the IC we want to comunicate is 3.3V logic level.
Regards, 
Khoa Tran.

Edit Notes

Fix the wrong VDDIO and VDDIOH
[edited by: KhoaTran12111992 at 7:24 AM (GMT -5) on 6 Mar 2024]