Post Go back to editing

Can the MAX32655 uses as just LC3 codec?

Thread Summary

The user inquired about using the MAX32655 as an LC3 codec for decoding and encoding LC3 data through UART and outputting PCM audio through I2S, without using other Bluetooth functions. The final answer directed the user to visit the Analog Devices technical support pages for further assistance, without confirming if the current SDK supports this scenario. No specific product alternatives were suggested.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX32655

Hi,

We would like to use MAX32655 as the just LC3 codec not uses any other BT function.
For decode case, LC3 data is comming from other dvice through the UART and it decoded by the MAX32655 then it output PCM audio through I2S.
For encode case, it opposit way, PCM data is comming from other dvice through the I2S and it encoded by the MAX32655 then it output LC3 data through UART.
Can we realize this scenario by using MAX32655 with current SDK?
If no, please suggest another ADI device?

Regards,
Suzuki