Post Go back to editing

RTIA, Calibration and Current

Category: Software
Product Number: AD5941

Hi, ADI Support.

I am having an issue with the AD5941, the problem I am facing is that when changing the RTIA (Gain Resistor) I am getting very different currents. I have noticed a ratio of 0.6 from the currents observed with the 1K and 200 Ohm gain resistors.

I am changing the code before initialization, not during the measurement. I have checked the currents with a multimeter and it is approximately the same as when I am using the 200 Ohm gain resistor.

Could you give me any insight into why this may be happening?

So essentially I would like to know if I should be observing the same current when switching Gain Resistors (RTIA) or should I see a reduction in current when moving to higher Gain resistor?

Thanks in advance.

Parents
  • Hi,

    Input to ADC of AD5491 = input current X RTIA

    This ADC input must be within +/-900mV (for PGA gain = 1 or 1.5)

    - As long as this input is within allowed range, there won't be any change in current measurement output with change in RTIA value.

    - If this input goes out of range (by changing RTIA value), output deviates due to saturation and hence gives different current output value which is not the actual input current value.

Reply
  • Hi,

    Input to ADC of AD5491 = input current X RTIA

    This ADC input must be within +/-900mV (for PGA gain = 1 or 1.5)

    - As long as this input is within allowed range, there won't be any change in current measurement output with change in RTIA value.

    - If this input goes out of range (by changing RTIA value), output deviates due to saturation and hence gives different current output value which is not the actual input current value.

Children
No Data