Post Go back to editing

MAX32670 SWD programming through CMSIS-DAP Error connecting DP: cannot read IDR

Category: Software
Product Number: max32670
Software Version: Eclipse MaximSDK August 7, 2022 Release

I have a MAX32670 on a custom board that I program with SWD using a DAP board that comes with most MAX326xx eval boards. We disconnect the DAP board from the eval board and solder the wires to a cable that connects to our board.

This has worked fine for a long time for us, but recently two of our MAX32670s have stopped programming this way. I can't see any good reason why this would happen. The CPU still boots up and runs the last firmware we downloaded to it just fine, and nothing unusual happened between the time they last programmed successfully and when they stopped, or at least nothing that I can identify.

We use the eclipse MaximSDK with a GDB OpenOCD debug configuration using these arguments in the debugger tab:

-s ${TOOLCHAIN_PATH}/OpenOCD/scripts -f interface/cmsis-dap.cfg -f target/max32670.cfg

We have also disabled the options "Enable Arm semihosting" and "Pre-run/Restart reset" in the Startup tab.

I see these messages when I try to run the debugger:

Open On-Chip Debugger 0.11.0+dev-g56a818e4c (2023-06-28-22:13)

Licensed under GNU GPL v2

For bug reports, read

openocd.org/.../bugs.html

DEPRECATED! use 'adapter driver' not 'interface'

DEPRECATED! use 'adapter srst delay' not 'adapter_nsrst_delay'

DEPRECATED! use 'adapter srst pulse_width' not 'adapter_nsrst_assert_width'

Started by GNU MCU Eclipse

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : CMSIS-DAP: SWD supported

Info : CMSIS-DAP: FW Version = 1.0

Info : CMSIS-DAP: Interface Initialised (SWD)

Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1

Info : CMSIS-DAP: Interface ready

Info : clock speed 2000 kHz

Error: Error connecting DP: cannot read IDR

All the messages except "Error connecting DP: cannot read IDR" are what I see normally.

I feel as though the chip has been locked and can no longer be programmed, but I don't see how that could have happened. Does anyone have any ideas?

Thanks



tagged
[edited by: GenevaCooper at 1:38 AM (GMT -5) on 31 Jan 2024]
Parents Reply Children
No Data