Post Go back to editing

Eval-ADuCM355 Interrupts in sample code are never executing

Category: Software
Product Number: ADuCM355
Software Version: aducm355-examples

Hey,

i'm trying to test the functionalities of the aducm355 with the code examples. I haven't modified the code in any way.

I tried the following code examples:

- Temperatur

- Impedance (for this sample i connected some resistors on the interface)

An interrupt should occur and data should be printed out, but as soon as the function "AD5940_GetMCUIntFlag()" get called the return value stays 0 all the time. So i guess the interrupt never occurs? 

Is this behaviour intended?  Do i have to modifiy the example code so the interrupt get executed? 

Thanks for any help

Shaheen

Thread Notes

Parents Reply Children