Post Go back to editing

"FVAL-ADICUP360 REV1.1" cannot be downloaded

Category: Hardware
Product Number: 114991707_1905 0000425
Software Version: FVAL-ADICUP360 REV1.1

help !!!

我的开发板插在电脑上后,会显示了一个MBED盘符

这种方式不能用MDK下载程序么?

并且显示这个MBED盘符后,大概每隔10秒钟重启一次,即断开盘又连接,感觉是这个开发板自带的下载器有问题

并且MDK中选择 CMSIS-DAP 也找不到设备,也无法下载。J3,J4都接上了也不行

通过 ISP命令发送0x8数据也无回应。

是不是我买的这个板子是坏的?这么不巧?

After my development board is plugged into the computer, an mbed drive letter will be displayed

Can't MDK download programs in this way?

After the mbed drive letter is displayed, restart it every 10 seconds, that is, disconnect and connect the drive. I feel that there is a problem with the downloader of the development board

In addition, if cmsis-dap is selected in MDK, the device cannot be found and cannot be downloaded. J3 and J4 can't be connected

There is no response to sending 0x8 data through ISP command.

Is this board I bought broken? So unlucky?

Hi xa87,

Can you please provide some more information about your issue?  What is MDK?  What exactly are you doing?  Do you have any pictures or screen shots you could send?

  • Thank you for your reply.

    MDK means keil

    This board will recognize a device named "CMSIS DAP" after it is inserted into the computer. But in fact, it is not in the device manager.

    There is only one USB drive with the display name "mbed", which will be constantly displayed and hidden.

    Can it be understood as a problem board?

  • Is anyone here? I really want to solve this problem.

    Thank you very much.

  • FormerMember
    0 FormerMember on Jul 29, 2022 10:57 AM in reply to xa87

    So I know those instructions are pretty old, but I'm sure it will work with Keil I am just not an expert when it comes to using that tool.

    My suggestion would be to download Cross Core Embedded Studio and try to install all the packs their and see if you can program the EVAL-ADICUP360 via that tool.  That is the fully supported and maintained tool we use here at Analog Devices.  This will give more insight as to what is happening.  One other thing to check on is the driver for the MBED drive itself, sometimes that is the root cause of this type of behavior.  (Windows serial configuration - Handbook | Mbed)

  • Reply
    • FormerMember
      0 FormerMember
    on Jul 29, 2022 10:57 AM in reply to xa87

    So I know those instructions are pretty old, but I'm sure it will work with Keil I am just not an expert when it comes to using that tool.

    My suggestion would be to download Cross Core Embedded Studio and try to install all the packs their and see if you can program the EVAL-ADICUP360 via that tool.  That is the fully supported and maintained tool we use here at Analog Devices.  This will give more insight as to what is happening.  One other thing to check on is the driver for the MBED drive itself, sometimes that is the root cause of this type of behavior.  (Windows serial configuration - Handbook | Mbed)

    Children
    No Data