help !!!
我的开发板插在电脑上后,会显示了一个MBED盘符
这种方式不能用MDK下载程序么?
并且显示这个MBED盘符后,大概每隔10秒钟重启一次,即断开盘又连接,感觉是这个开发板自带的下载器有问题
并且MDK中选择 CMSIS-DAP 也找不到设备,也无法下载。J3,J4都接上了也不行
通过 ISP命令发送0x8数据也无回应。
是不是我买的这个板子是坏的?这么不巧?
After my development board is plugged into the computer, an mbed drive letter will be displayed
Can't MDK download programs in this way?
After the mbed drive letter is displayed, restart it every 10 seconds, that is, disconnect and connect the drive. I feel that there is a problem with the downloader of the development board
In addition, if cmsis-dap is selected in MDK, the device cannot be found and cannot be downloaded. J3 and J4 can't be connected
There is no response to sending 0x8 data through ISP command.
Is this board I bought broken? So unlucky?