Post Go back to editing

Migrating from ADuCM360/1 to 362/3

I can flash the codes written for 360/1 to 362/3 and the program actually runs, but the ADC reading is wrong. It is about 3 times higher than it should be.

Based on https://www.analog.com/media/en/technical-documentation/frequently-asked-questions/differences-aducm360-aducm362-faqs.pdf, there is difference in ADCxCFG (from 2 bits to 3 bits),

Based on 360/1 definition files, we have

/* ADCCON[BUFBYPN] - Negative buffer bypass */
#define ADCCON_BUFBYPN_MSK (0x1 << 14 )
#define ADCCON_BUFBYPN (0x1 << 14 )
#define ADCCON_BUFBYPN_DIS (0x0 << 14 ) /* DIS */
#define ADCCON_BUFBYPN_EN (0x1 << 14 ) /* EN */

/* ADCCON[ADCREF] - Reference selection */
#define ADCCON_ADCREF_MSK (0x3 << 12 )
#define ADCCON_ADCREF_INTREF (0x0 << 12 ) /* INTREF */
#define ADCCON_ADCREF_EXTREF (0x1 << 12 ) /* EXTREF */
#define ADCCON_ADCREF_EXTREF2 (0x2 << 12 ) /* EXTREF2 */
#define ADCCON_ADCREF_AVDDREF (0x3 << 12 ) /* AVDDREF */

I would like to change it to reflect the difference of 362/3. Unfortunately, I can't find the definition of ADCxCFG of 362/363. When I visit https://www.analog.com/media/en/technical-documentation/user-guides/ADuCM36x-Getting-Started-Tutorial-UG-1063.pdf, there is ONLY 360/361 user guide, but not 362/3 guide to see what I can change to

Can i have some pointers? Thanks!

Parents Reply Children
No Data