Post Go back to editing

ADuCM355 32MHz Crystal

Thread Summary

The user is seeking the part number for a 32MHz crystal used on the EVAL-ADuCM355QSPZ development board. The final answer identifies the crystal as an EPSON TOYOCOM FA-128, 32MHz, 10PPM, 8pF. However, a 16MHz crystal like the ABRACON ABM8-16.000MHZ-7-1-U-TCORP is recommended for most applications due to lower power consumption, especially since the ADuCM355 AFE die runs at 16MHz by default and only uses 32MHz for impedance measurements at frequencies >=80kHz.
AI Generated Content

Hello!

I'm working with the ADuCM355 IC and would like to use the same 32MHz crystal as on the EVAL-ADuCM355QSPZ development board for my design.  I cannot find the part number in any of the documents, but the package is labeled: 3200P E9318.

Can you share what this crystal is?  Thank you!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.