Post Go back to editing

ADuCM360 Internal Difference Amplifier for current sensing

I have a ADuCM360 using which i would like to monitor the voltage across a 100mOhm current sense resistor. Is it possible to connect the two terminals of the resistor directly to the MCU ? E.g. current in terminal to AIN0 and current out terminal to AIN1 ? Will the internal differential amps detect the voltage difference across the resistor ?

(Assuming the current is not exceeding 500mA)

  • Hi,

    Yes you can use ADuCM360 to monitor voltage for your current sense resistor however you have to protect the input pins if your passing a huge amount current.

    Please be aware of the ADC input current which can cause some drift on your measurement. You will find the input current values for Buffered and Unuffered Mode on page 7 of ADuCM360 Rev C datasheet. You'll also find the ADC input current for different Common Mode Voltages on figures 9 and 10 on page 22 of ADuCM360 Rev C datasheet.

    Regards,

    Mark

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.