Post Go back to editing

ADuCM355 Using AFE Clock for Digital Die

Thread Summary

The user encountered an issue where the MCU stopped responding when trying to enable the 32MHz HFSOC of the AFE die to increase processing speed. The final answer clarifies that the digital die's maximum clock rate is 26MHz and provides the required clock ratio between the AFE and digital die (3:1 to 1:3) to maintain reliable communication. The user should ensure the clock settings are within these limits.
AI Generated Content

Hi,

Based on UG-1262 Rev A. page 14, the Digital Die can use the clock of AFE die. I am trying to use the 32MHz HFSOC of AFE die to further increase the processing speed. While trying to activate this feature, CLK CTL0[1:0] = 0x03, the MCU stops responding. Can you guide me on the proper sequence to enable this?

Thanks.

  • Hi Yan-Wei,

    A couple of points to note:

    - The digital die maximum clock rate is 26MHz. This is the max clock rate the memories and digital logic were tested and qualified to. 

    - Did you follow the steps in the user guide under the section "Connecting AFE Die clock to Digital die clock input"?

    - Also note the clock ratio requirement between the AFE and digital die - see following from the user guide:

    REQUIRED CLOCK RATIO BETWEEN DIGITAL DIE AND ANALOG DIE SYSTEM CLOCKS
    To maintain reliable communications between the digital die and the analog die, the ratio of the digital die system clock frequency to the analog die system clock frequency must be within the range of 3:1 and 1:3. For example, if the digital die system clock is set to 6.5 MHz, the analog die system clock must be >2.2 MHz but <19 MHz. If this ratio is not maintained, the digital die can lose its communication link to the analog die.

    Regards,

    Mike

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.