ADuCM330
Not Recommended for New Designs
The ADuCM330 is a fully integrated, 8 kSPS, data acquisition system that incorporates dual, high performance multichannel sigma-delta (S-?) ADCs, 32-bit...
Datasheet
ADuCM330 on Analog.com
Hi team,
My customer would like to develop e-scooter as end-product. Now they are focus on the BMS portion and battery specification as below.
Rated voltage: 60V
Rated Capacity: 29Ah
Battery Configuration: 16S1P
Could you propose a solution / application with ADI?
How we apply ADUCM330 into BMS circuit?
Customer is looking at the swap battery type but not charging the battery directly onto the E-scooter. Refer to https://electrek.co/2019/09/23/check-out-gogoros-giant-new-battery-swap-stations-for-its-electric-scooters/
Looking forward the guide.
Thanks
John
Hi John,
the ADuCM330 was developed with primary focus on 12V Lead Acid Battery management.
However, the ADuCM330 is also used in LI-Ion battery management systems for precision current measurements, which I assume is the application you are interested in.
Please refer to the recommenced schematics in the ADuCM330 datasheet.
regards
Holger