Post Go back to editing

Debugging hardware needed??

FormerMember
FormerMember

Do I need any external debugging hardware in order to use the ADuCM360 IDE and the ADICUP360? (ie Segger J-Link)

Parents
  • FormerMember
    0 FormerMember
on Feb 5, 2016 5:55 PM

You do not need any external hardware tools in order to download or debug the ADICUP360 board when using the ADuCM360 IDE.

All the debug hardware is on the ADICUP360 board, making it simple and easy to connect and develop without the expensive debug tools.  Simply plug in the ADICUP360 board using the"DEBUG" USB port, and start developing your code in the ADuCM360 IDE.

Cheers,

Brandon

Reply
  • FormerMember
    0 FormerMember
on Feb 5, 2016 5:55 PM

You do not need any external hardware tools in order to download or debug the ADICUP360 board when using the ADuCM360 IDE.

All the debug hardware is on the ADICUP360 board, making it simple and easy to connect and develop without the expensive debug tools.  Simply plug in the ADICUP360 board using the"DEBUG" USB port, and start developing your code in the ADuCM360 IDE.

Cheers,

Brandon

Children
No Data