Post Go back to editing

How to use a J-LINK with ADICUP360

I have been working with the ADICUP360. Awesome tool! I have progressed to where I need to connect the board to my J-LINK probe and am having trouble. I see from the schematics that the 10-pin Cortex debug connector P16 connects to the M360 SWD pins, but also to the on-board SDA interface. How han I force the SDA interface to relinquish contol and allow the J-LINK to control the SWD pins?

Thanks in advance!

Parents
  • FormerMember
    0 FormerMember

Hi Steven,

Glad to hear you like the ADICUP360 board

So I'm a bit curious as to why you are using a J-Link to attach to the ADICUP360.   There is an on board debugger/programmer for you to use, which connects directly to the USB port of your PC.

There is also a way to directly load the on board programmer with a binary or hex file, and you can simply drag and drop the file you wish to load via the "MBED" drive that shows up as a removable drive.

Which tool chain are you using?  We provide a set of tools with instructions which can be used with the ADICUP360.  You can find all those details and many more up here on our user guide.

Cheers,

Brandon

Reply
  • FormerMember
    0 FormerMember

Hi Steven,

Glad to hear you like the ADICUP360 board

So I'm a bit curious as to why you are using a J-Link to attach to the ADICUP360.   There is an on board debugger/programmer for you to use, which connects directly to the USB port of your PC.

There is also a way to directly load the on board programmer with a binary or hex file, and you can simply drag and drop the file you wish to load via the "MBED" drive that shows up as a removable drive.

Which tool chain are you using?  We provide a set of tools with instructions which can be used with the ADICUP360.  You can find all those details and many more up here on our user guide.

Cheers,

Brandon

Children
No Data