Post Go back to editing
Captured to Debug Board needed wiki page

Debug Board needed

Dear sir,

I am Sunil, Student at IIT bombay using ADuC360 in my board. so Is it possible to procure J Link SWD Debugger to debug/program in my board. If not, Can you suggest any third party SWD debuggers which can be used to program  ADuC360..

Thanks

Sunil

Parents
  • FormerMember
    FormerMember
on Jun 9, 2016 2:31 PM

You should be able to use the standard Jlink Segger board (either base or student version) to program the ADuCM360.  However you will not be able to use the Analog Devices Eclipse IDE we provide, as it is set up to work with the EVAL-ADICUP360 board

If you are using the Jlink Segger SWD for your board, then you will want to use Keil or IAR program to program and debug the board (easiest way).  You should be able to find trial versions of both those programs on their respective websites.

Brandon

Reply
  • FormerMember
    FormerMember
on Jun 9, 2016 2:31 PM

You should be able to use the standard Jlink Segger board (either base or student version) to program the ADuCM360.  However you will not be able to use the Analog Devices Eclipse IDE we provide, as it is set up to work with the EVAL-ADICUP360 board

If you are using the Jlink Segger SWD for your board, then you will want to use Keil or IAR program to program and debug the board (easiest way).  You should be able to find trial versions of both those programs on their respective websites.

Brandon

Children
No Data